To achieve access level 4 in Tracer TU; when connected to a chiller with UC800 controls:
- Select the wrench tab on the right side to view the unit setpoints and configuration menus.
- Select the Field Startup tab.
- Locate the grey bar at the bottom of the screen. This grey bar also contains the "save" and "cancel" buttons.
- Left mouse click on the LEFT END of the grey bar. The left area of the grey bar is blank, but the level 4 button is hidden in this area.
The level 4 setpoints should now be visible above in the "Field Startup" menus.
Notes
Can't see the level 4 access drop down boxes?
- If your laptop is a touchscreen, try touching the screen vs using the mouse pad.
- If not, try increasing the screen resolution on your PC.
Right click our our desktop, then select Display Settings.
Then, under Scale & Layout, change the size of text and the Resolution to the recommended values.
Additional details
Other Question/Problem/Cause Statements
- Tracer TU Access Level 4
- How do I achieve a level 4 access level for Tracer TU?
- Where do I set starts and hours with Tracer TU?
Facts
- UC800