Does the LCI-C LonTalk card come programmed from the factory?
When adding a LonTalk LCI-C module that was not factory installed it will come programmed for CTV extension. Therefore, when field adding this option to RTAC Chillers, the Techview Service Tool and Rover Software will be needed. Techview Service Tool will be needed to be introduce the Main Processor (Dynaview) to the module through the binding procedure. Also, Rover service tool will be needed to flash download the correct Neuron software to the LCI-C. Detailed procedures can be found in the installation guide ACC-SVN25D-EN (or latest revision) starting in the "Hardware and Software Installation Section" of the bulletin.
Additional details
Other Question/Problem/Cause Statements
- Does the LCI-C Lon talk card come programmed from the factory?
- How do I program Lon Talk for the chiller using extended profile?
- Does the RTAC use profile only or extension on RTAC Chillers?
Facts
- Pueblo Screw and Scroll
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.