What is the RTHB tube size?
- The RTHB condenser uses 0.75 inch (19.0 mm) outside diameter copper tubes.
- The standard tube has a nominal bottom wall thickness of 0.026 inch (0.6604 mm).
- The smooth bore and CuNi smooth bore tubes have a minimum bottom wall thickness of 0.035 inch (0.889 mm).
- The RTHB evaporator uses 1.0 inch (25.4 mm) outside diameter copper tubes. The tube has a nominal wall thickness and bottom wall thickness of 0.028 inch (0.7112 mm).
- Standard tubes are externally finned, internally enhanced seamless copper with lands at all tube sheets.
- The tubes can be individually replaced.
Additional details
Other Question/Problem/Cause Statements
- What is the evaporator tube diameter?
- What is the condenser tube diameter?
- What is the OD for this tube?
- What is the ID for this tube?
- What is the inside diameter of the tube?
- What is the outside diameter of the tube?
- What is the tube wall thickness?
- What is the nominal wall thickness?
- What is the bottom wall thickness?
- What is the RTHB tube size?
Facts
- Water-Cooled Chiller (Pueblo) (RTHB)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.