Pueblo manufacturing has now introduced BCI2-C for Pueblo products with CH530 controls. Current manufactured products will include RTAC, RTWD, and CGAM units.
Please see:BCI-C for Pueblo Chillers for details regarding chiller design sequence and which LLID (UC400, Reliatel BCI-R, and BCI2-C) was originally installed in the unit from the factory.
Design Sequence drives the type of BCI-C module/LLID in a chiller; (BCI2-C)
The unit design sequence are digits 10 and 11 of the unit model number.
- RTAC Design Sequence 1L and newer
- CGAM Design Sequence X0 and newer
- RTWD / UD Design Sequence M0 and newer
-
RTAC, CGAM, RTWD, and RTUD chillers selected with the BCI-C interface as an option from the factory will now have the BCI2-C module installed, configured as a BCI-C
BCI2-2 Field Installation requires KIT19852 which includes the following:
- BCI2-C LLID
- Cable
-
Bracket (2X)
Installation Pictures for Reference Only
Reference the appropriate service literature for details. See the links below.
- also visit E-Library for the latest revisions
Notes
- The chiller can use BAS, Local or external setpoints
- Change the "Setpoint Source" on the Chiller DynaView to 'BAS' to be able to control from Tracer SC/SC+ or a third party BAS
Additional details
Reference Literature
- BAS-SVP055A-EN BCI2-C Integration Guide
- RF-SVN006C-EN BCI2-C Installation Instructions
- Other: See BCI2 Web UI, Board Overview, Changing Device ID and LEDs
Other Question/Problem/Cause Statements
- BCI
- BACnet
- BCI-C
- BCI-R
- BCI2-C
Facts
- Air-Cooled Chiller (Pueblo)
- Water-Cooled Chiller (Pueblo)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.