Is this Modbus compatible?
Pueblo chillers with a CH530, UCP2 or UCM controller are not capable of interfacing directly with Modbus, except via hardwire points. The chillers are able to interface directly with Lontalk, hardwire points, and Tracer Summit. Chillers with a CH530 controller can also interface directly with BACnet MS/TP. Once points are passed to Tracer Summit, the Summit package can be capable of communicating with Modbus.
For chillers with CH530 controls, one solution would be to communicate Lontalk to a "Babel Buster" gateway.
- Controls Solutions Minnesota
- LonWorks to Modbus Gateway: Babel Buster BB2-2010-NB
- LonWorks to Modbus TCP Gateway: Babel Buster BB2-6020-NB
The new RTAE Stealth chiller and the RTHD Optimus chiller both have a UC800 controller. This controller has the ability to communicate Lontalk, BACnet MS/TP and ModBus RTU protocols.
Additional details
Other Question/Problem/Cause Statements
- Is this Modbus compatible?
- Are Pueblo chillers able to interface directly with Modbus?
- Can this chiller communicate with Modbus directly?
- How can I comply with the requirement for Modbus communication?
- The job requires Modbus communication, what do I need to order with the chiller to meet this?
Facts
- Air-Cooled Chiller (CGA, 10-15 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Air-Cooled Condenser (Pueblo) (RTCA)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Compressor Chiller (Pueblo) (CCAF)
- Water-Cooled Chiller (Pueblo) (CGWF)
- Water-Cooled Chiller (Pueblo) (RTWD)
- Air-Cooled Chiller (Pueblo) (RTAE)
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.