Can damaged tubes be plugged in evaporator and condenser?
Yes, it is possible to plug leaking tubes. Make sure that no more than 10% of the tubes are plugged.
Additional details
Other Question/Problem/Cause Statements
- Can leaking tubes be plugged in a DX evaporator?
- Evaporator tube leak repair?
Facts
- RTWA
- Air-Cooled Chiller (CGAA)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Evaporator Chiller (EVP)
- Water-Cooled Chiller (PBL) (CGWA, CGWB, CGWC, CCAA, CCAB, CCAC)
- Water-Cooled Chiller (PBL) (CGWD, CGWE, CGAD, CGAE, CCAD, CCAE)
- Water-Cooled Chiller (Pueblo) (CGWF, CCAF)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.