Are the inlet and outlet refrigerant lines on a braze plate heat exchanger crisscrossed?
It depends on the Design Sequence of the chiller (Digit 10 in the model number).
For "K" Design Sequence:
This heat exchanger was made by Alfa Laval. The refrigerant lines are crisscrossed. The liquid line (on the bottom) and the suction line (on the top) are not directly over one another for an individual circuit. The liquid lines are crisscrossed on a dual circuit unit. The TXV sensing bulb and equalizer lines should also follow the refrigerant lines.
For "L" Design Sequence and higher:
This heat exchanger was made by SWEP. The refrigerant lines are not crisscrossed. The liquid line (on the bottom) and the suction line (on the top) are directly over one another for an individual circuit. The TXV sensing bulb and equalizer lines should also follow the refrigerant lines.
Additional details
Other Question/Problem/Cause Statements
- Are the inlet and outlet refrigerant lines on a braze plate heat exchanger criss-crossed?
Facts
- INTELLIPAK CHILLER 20-60
- Air-Cooled Chiller - Intellipak (CGAF)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.