Copper to Copper
- BCuP6 (2%silver) without flux. It contains Phosphorous. This is an alloy that is self fluxing, no flux is required.
Copper to Brass
- BCuP with flux or BAg28 (40% silver) with flux. The oxide on the brass is heavier than that of the copper, flux is needed.
Copper to Steel
- BAg28 (40% silver) with flux. 40% silver alloy is used because of its low brazing temperature and free flow characteristics.
Additional details
Other Question/Problem/Cause Statements
- Brazing Filler Material
Facts
- Air-Cooled Pueblo
- Water-Cooled Pueblo
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.