Discussion
UCP2 Solid State Starter Faulty Relay Open diagnostic was active in ALL modes. If the Starter Drive Fault Input is found to be opened, J7-3 to J7-4 while UCP2 Controls are powered, the latching diagnostic Solid State Starter Faulty Relay Open will lock-out the chiller. A manual Reset will need to be performed, even though the chiller was never operating. This diagnostic was present in ALL previous versions of UCP2 Software.
Solution
Problem was corrected in the -22 starter module (X13650453-22, MOD01232, Rev. AG). If you experience this problem, replace the UCP2 Starter Module.
Notes
- This problem could affect UCP2 starter modules on Centra Vac and Screw Chillers.
- If the Starter Fault Input opens during an MPL or Power Loss before the Controls shut down (2-3 seconds), this diagnostic would be active and lock out the chiller.
Additional details
Other Question/Problem/Cause Statements
- Solid State Starter Faulty Relay Open...UCP2
- Power Loss or Momentary Power Loss while chiller is in Standby or Auto...waiting for need to cool
- MPL
- Power Loss
- Loss of Power
Facts
- RTHC (PUEBLO)
- CenTraVac - Direct Drive Duplex (Taicang) (CDHF, CDHG)
- CenTraVac - Direct Drive Simplex (CVHE, CVHF, CVHG)
- CenTraVac - Gear Drive (CVGF)
- Water-Cooled Chiller (Pueblo) (RTHC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.