The waterside pressure rating for all Pueblo products can be found in the products's catalog, under "Mechanical Specifications".
Air Cooled
| Chiller model | Evaporator / Heat Exchanger | Water Side working pressure rating (psig) |
|---|---|---|
| ACRA | Evaporator | 150 |
| ACSA | Evaporator | 150 |
| RTAC | Evaporator | 150 |
| RTAE | Evaporator | 150 |
| RTAF | Evaporator | 150 |
| CGAM | Evaporator | 150 |
| CGAF | Braze Plate Heat Exchanger | 300 |
| CGA | Braze Plate Heat Exchanger | 350 |
Water Cooled
| Chiller model | Evaporator / Condenser | Water Side working pressure rating (psig) |
|---|---|---|
| RTHD | Evaporator & Condenser | 150 (option for 300 psig) |
| RTHB | ||
| RTWD | Evaporators & Condenser | 150 |
| RTUD | Evaporator | 150 |
| RTWA | Evaporator | 215 |
| Condenser | 150 | |
| RTUA | Evaporator | 215 |
| RTAA | ||
| CGWF060 | Evaporator | 215 |
| Condenser | 150 | |
| RTWA | Evaporator | 215 |
| CGWF 20-50 | Evaporator & Condenser | 300 |
| CCAF 20-60 |
Unless noted, there is not an option for a different water side pressure rating.
Notes
- Literature can be found in E-Library
Additional details
Other Question/Problem/Cause Statements
- Water side working pressure ratings
- Can the waterside be rated for 450 psi?
- Can we get a larger waterside rating?
- Can the water boxes be rated for higher pressure?
- What is the waterside pressure rating for RTWA evaporators?
Facts
- Air-Cooled Chiller (Pueblo) (ACRA 150-300 Ton)
- Air-Cooled Chiller (Pueblo) (ACSA 140-230 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC 140-500 Ton)
- Air-Cooled Chiller (Pueblo) (RTAE 150-300 Ton)
- Air-Cooled Chiller (Pueblo) (RTAF 115-520 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Air-Cooled Chiller (CGA, 10-15 Ton)
- Compressor Chiller (Pueblo) (RTUD 70-200 Ton)
- Water-Cooled Chiller (Pueblo) (RTWD)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.