Failed "Advance, Stop/Reset-Auto Local/Remote, Service/Operating Menu" switch/button. Micro works, but one or more of the following Buttons; "advance," "Stop/Reset," "Auto Local/Remote," "Service/Operating Menu" is not working. Typical repair would be to replace the micro. The switch(s) can be purchased through the following distributors; and can be replaced at a local TV or micro-electronic repair shop. This is a circuit board/component level repair. Appropriate tools (solder iron), and steps for handling static sensitive devices should be followed.
Advance Display
- Part Number: PS8-131B
- Manufacturer: Electroswitch Electronic Products
Stop/Reset, Auto Local/Remote
- Part Number: B121J71V3B2
- Manufacturer: Electroswitch Electronic Products
Service/Operating Menu
- Part Number: B123J71V3B2
- Manufacturer: Electroswitch Electronic Products
Manufacturer
- Electroswitch Electronic Products
2010 Yonkers Road Raleigh, NC 27604 USA
888-768-2797 or 919-833-0707
www.electroswitch.com
Distributors
Digi-Key
701 Brooks Avenue South Thief River Falls, MN 56701
800-344-4539Newark Electronics
4801 N. Ravenswood Chicago, IL 60640
800-367-3573
Additional details
Other Question/Problem/Cause Statements
- Advance Display, Stop/Reset / Auto Local / Auto Remote Switch/Button Repair
- Display switches do not work?
- Push button switches on display not functioning.
Facts
- Water-Cooled Chiller (PBL) (CGWD, CGWE, CGAD, CGAE, CCAD, CCAE)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.