Clear Language Display (CLD) not working.
ALL Clear Language Displays on RTAA, RTWA, RTUA, RTHB, RTHC, CTV & CentraVac chillers with Adaptive Controls 1.5 or UCP2 controls.
To enter the CLD Demo mode:
- Disconnect the IPC communication link from the CLD
- Remove power from the CLD
- Press the ' Custom Report ' and ' Compressor Report ' buttons simultaneously (at the same time) while the display is powering up. (Note: The CLD will not enter the demo mode if these keys are pressed after power is applied.)
- Demo mode will allow you to go through ALL menu items in the CLD without effecting the chiller controls.
- To EXIT Demo mode: If the CLD hears from the Chiller module, it will exit the demo mode; to exit Demo Mode simply reconnect the IPC link or power down and reconnect the IPC link (then reapply power).
To enter the CLD Test mode:
- Disconnect the IPC communication link from the CLD
- Remove power from the CLD
- Press the ' Next ' and ' + ' buttons simultaneously (at the same time) while the display is powering up. (Note: The CLD will not enter the Test mode if these keys are pressed after power is applied.)
- Follow instructions on the CLD 2-line display by pressing ' Next ', ' - ', ' Cancel ', and ' Stop ' to advance to the desired test:
- ' Next ' >>> Execute
- ' - ' >>> Skip
- ' Cancel ' >>> Exit
- ' Stop ' >>> [ intentionally left blank ]
- Test mode allows a lower level test of each key and CLD 2-line LCD segment and pixels.
- To EXIT Test mode: If the CLD hears from the Chiller module, it will exit the Test mode; to exit Test Mode simply reconnect the IPC link or power down and reconnect the IPC link (then reapply power).
Notes
- This information is applicable to ALL Clear Language Displays used on RTAA, RTWA, RTUA, RTHB, RTHC, CTV & CentraVac chillers with Adaptive Controls 1.5 or UCP2 controls.
Additional details
Other Question/Problem/Cause Statements
- CLD Test Mode
- CLD DEMO Mode
- Clear Language Display testing
- HI not working
- Human Interface not working
- Human Interface not functioning
- CLD not working
- Failed Human Interface
- Failed CLD
- Failed Clear Language Display
- CLD Testing?
- How to test a CLD?
- How to test a Clear Language Display?
Facts
- Water-Cooled Chiller (Pueblo) RTHB, RTHC
- Water-Cooled Chiller (La Crosse) CentraVac and CTV using UCP2
- Air-Cooled Chiller (Pueblo) RTAA, RTWA, RTUA using Adaptive Controls 1.5
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.