Diagnostic: Starter Fault Type I
Source: Starter
Active Period: Starting Compressor (YDelta Starters Only)
Severity: Immediate Shutdown
Persistence: Latching
Description of Trigger Behavior: The 'Starter Contactor Integrity Test' was enabled, and greater than 10% RLA was detected on one or more of the CT inputs when only the 1M contactor was commanded to pull in.
Troubleshooting Guide:
This is a specific starter test where the 1M contactor is closed first and acheck is made to ensure that there are no currents detected by the CT's. If currents are detected when only 1M is closed first at start, then one of the other contactors is shorted or there exists a wiring error.
Additional details
Other Question/Problem/Cause Statements
- Starter Fault Type I; CH530
Facts
- CDHF, CDHG
- CVGF
- CVHE, CVHF, CVHG
- RTAC
- RTHD
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.