RTAA, RTWA, RTUA, RTHB/C/D, RTWD, RTUD, CGAM Chillers
-
RTAA, RTWA, RTUA Chillers:
- These chillers have the ability to start and stop the chilled water pump, but it is not required
-
RTHB, RTHC, RTWD, RTHD Chillers:
- These chillers have the ability to start and stop the chilled water pump, but it is not required
-
CGAM Chillers:
- These chillers have the ability to start and stop the chilled water pump, but it is not required.
- Units with factory installed pump package require pump control.
-
RTAC Chillers:
- These chillers have the ability to start and stop the chilled water pump, but it is not required.
- Freeze Avoidance and Pump Control Requirements
-
RTUD Chillers:
- These chillers have the ability to start and stop the chilled water pump
- Is pump control mandatory for the RTUD chiller?
RTAA, RTWA, RTUA, RTHB/C/D, RTWD, RTAC, CGAM Chillers
Flow Proving
-
RTAA, RTWA, RTUA Chillers:
- Proof of Flow is required for all Pueblo built chillers; however flow switches are not required on for RTAA, RTWA, RTUA Chillers.
-
RTHB, RTHC, RTHD, RTWD (when the factory installed flow switch is NOT selected) Chillers:
- Two forms of flow proving are REQUIRED.
- AUX Contacts off of the Pump Starter AND a Flow Proving Device (Paddle Flow Switch, DP Switch, Flow Proving Contact from BAS System, etc.,..)
- The two forms of flow proving are wired in Series configuration.
- Click here for reference...
- Are flow switches required for both the evaporator and condenser water loops? (RTHD)
- Is an external flow switch required? (RTHC)
-
RTAC Chiller
- A secondary set of pump interlocks. is strongly recommended, but not required.
-
CGAM Chillers
- A secondary set of pump interlocks is strongly recommended, but not required.
Additional details
Other Question/Problem/Cause Statements
- Chilled water flow interlock and flow switch
- Do I need to order a flow switch with my chiller?
- Pump Control and Flow Proving?
- Is pump control required for this chiller?
- Pump Control?
- Flow Proving?
- Flow Switch?
- Proof of Flow?
- Proof of Flow Requirements?
- Is a flow switch required for this chiller?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTWD)
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.