What is the acceptable moisture level in the oil and refrigerant?
Maximum moisture levels in the refrigerant circuit will need to be confirmed through both an oil sample and refrigerant sample. Values for chillers with Mineral Oil and R22 refrigerant will be different than those which contain POE and R134a.
See below for specifications:
RTAA, RTHA, RTHB, RTWA:
- The moisture level in the refrigerant must be below 50 PPM.
- The moisture level in the oil must be below 50 PPM.
RTAC, RTHC, RTHD, RTWD:
- The moisture level in the refrigerant must be below 50 PPM.
- The maximum moisture level in the oil must be below 300 PPM.
CGAM:
- The maximum moisture level in the oil must be below 100 PPM
- Acid level less than 0.5 TAN
Additional details
Other Question/Problem/Cause Statements
- What is the acceptable moisture level in the oil and refrigerant?
Facts
- Air-Cooled Chiller (Pueblo)
- Water-Cooled Chiller (Pueblo)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.