Where is the best place to take an oil sample?
The best place to pull an oil sample to be sent out for analysis is from the oil separator of the circuit or chiller. The sample should be in sealed container and sent off as soon as possible.
Standard practice is to send oil analysis samples in a sealed glass container; however, this can result in samples being lost or destroyed. Samples may be sent in a sealed plastic container; however the samples need to be sent and processed ASAP so contamination does not occur while using plastic containers.
Notes
- A secondary place to pull the oil would be off the bottom of the compressor once it has been isolated.
- If a customer is trending a chiller; ALL samples need to be taken from the same location.
Additional details
Other Question/Problem/Cause Statements
- Where is the best place to take an oil sample.
Facts
- Air-Cooled Chiller (Pueblo)
- Water-Cooled Chiller (Pueblo)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.