How can I disable the 2nd compressor on each circuit?
CGWD, CGWE, CCAD, CCAE, CGAD, CGAE Chillers: Cyclone Control
There is an input on the 1U1A1 which is called the Compressor Inhibit/KW Limit. This input is designed to accept an optional, field installed, isolated set of contacts to be used for compressor inhibit. The unit ships from the factory with a jumper installed between these terminals (TB1-1 and TB1-2). In the jumpered state, or when the attached contacts are closed, the UCM will operate the compressor under its normal algorithm. When this input is open, the UCM prevents the second compressor of each circuit from starting, or it will shut down the second compressor of each circuit, if running.
Additional details
Other Question/Problem/Cause Statements
- How can I disable the 2nd compressor on each circuit?
- How to lock out the second compressor on a circuit?
- Can I lock out the first compressor on a circuit?
- Can I lock out the larger compressor on a circuit?
Facts
- CGWD, CGWE
- Air-Cooled Chiller (PBL) (CGAD, CGAE)
- Compressor Chiller (PBL) (CCAD, CCAE)
- Water-Cooled Chiller (PBL) (CGWD, CGWE)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.