There were RAM errors detected in RAM Address Test #1 or #2.
Cycle power, if the problem persists:
- Replace the MP ( load new software )
- If a new MP does not help; replace the DynaView
Additional details
Other Question/Problem/Cause Statements
- Err2: RAM Pattern 1 or 2 Failure?
- Err2: RAM Pattern 1 Failure?
- Err2: RAM pattern 2 Failure?
Facts
- RTAC
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Compressor Chiller (Pueblo) (CCAF)
- Compressor Chiller (Pueblo) (RTUD 70-200 Ton)
- Water-Cooled Chiller (Pueblo) (CGWF)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWD)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.