RTHC and RTHB Chillers: UCP2 Controls
- RTHB
- Verify the jumper is installed from J3-1 to J3-2 on the 2U1 starter module.
- Make sure the electrical connections are good on J3-1 and J3-2.
If the above is ok, then replace faulty 2U1 starter module.
Notes
- This solution is applicable to ALL UCP2 controls.
Additional details
Other Question/Problem/Cause Statements
- Phase Sequence Monitor: Phase Reversal
- Phase Loss
- Phase Reversal
- Starter: Loss of Communication with Chiller
- RTHB-SB-3
- Phase Sequence Monitor: Phase Reversal?
Facts
- Water-Cooled Chiller (Pueblo) (RTHB)
- Packaged unit, NO remote starter
- Chillers built prior to March 1996
- RTHC (PUEBLO) Diagnostic occurs randomly about every two weeks. Phase Sequence Monitor input is jumpered (J3-1 to J3-2) on the starter module.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.