RTC Mismatch - all DynaView (CH530) controlled chillers.
- If the main processor halts operation, and there is a difference between the real-time clock ( RTC ) and oscillator, a diagnostic will be annuciated to show a failure.
- The chiller firmware checks the difference between the real time clock ( RTC ) and the microprocessor clock
- If it is off by a certain amount of time, in seconds ( 70 seconds ); then the controls annunciate the RTC Mismatch diagnostic.
Solution
- This diagnostic suggests that the microprocessor in the DynaView is locking up; which can lead to catastrophic failure.
- Recommendation is to replace the DynaView Controller.
Additional details
Other Question/Problem/Cause Statements
- RTC Mismatch
- "Unknown Diagnostic - 0X00010700"
- Unknown Diagnostic - 0X00010700
- CH530 locking up
- Unknown DynaView diagnostic
Facts
- Water-Cooled Chiller (Pueblo)
- Air-Cooled Chiller (Pueblo)
- CH530
- DynaView Display
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.