At what value should the low pressure switch open?
RTAA, RTWA, RTUA 70-125 TON Chillers:
- The low pressure switch is a normally OPEN switch which should open when the refrigerant charge in the circuit is at 7 psig or lower (+/- 10%).
- For low pressure diagnostics:
- Verify charge
- Could be a bad switch or schrader
- EXV not opening
Low pressure switch is installed on a Schrader valve
Additional details
Other Question/Problem/Cause Statements
- What should the low pressure switch open at?
- Low pressure cutout.
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.