What size are the vent and drain plugs?
- Drain and vent plugs are 1/2" 14 NPT
- They are located on the water boxes
- See the attached pictures for details
Additional details
Other Question/Problem/Cause Statements
- What size are the vent and drain plugs?
- Drain plug
- Where is the drain?
- Can the water be drained from the condenser and evaporator?
- What is the spec on the drain plug?
- What is the vent plug size?
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWD)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.