How do I bind a LLID?
CH530 Controls
- Connect to chiller using Techview
- Once connected with the appropriate Service tool select Binding View.
- Once in Binding View, search for the device(s) that need to be bound.
- Select Bind for the device desired.
- The question: Is the Desired Device Alone Selected? will display on the screen.
- Place a South Pole Magnet on the desired LLID, at the Dimple (Frame Mounted LLID) or White Arrow (Panel Mounted LLID) to select that LLID. A GREEN LED will light.
- Press Yes to the question Is the Desired Device Alone Selected?
- Device Status should change from RED (unbound) to GREEN (bound).
UC800/Symbio Controls
- Connect to chiller using Tracer TU
- Once connected with the appropriate Service tool select Binding View.
- Once in Binding View, search for the device(s) that need to be bound.
- Select Bind for the device desired.
- A popup showing Activate LLID using magnet and click OK will display on the screen.
- Place a South Pole Magnet on the desired LLID, at the Dimple (Frame Mounted LLID) or White Arrow (Panel Mounted LLID) to select that LLID. A GREEN LED will light.
- Press Yes to the question Is the Desired Device Alone Selected?
- Device Status should change from RED (unbound) to GREEN (bound).
Notes
- See appropriate IOM and Troubleshooting Service Bulletins for additional reference.
Additional details
Other Question/Problem/Cause Statements
- How do I bind a LLID?
- Binding Problems?
- Binding?
- Bind?
- Can not get device to bind?
- How do I bind a device?
Facts
- Air-Cooled Chiller (Pueblo)
- Water-Cooled Chiller (Pueblo)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.