RTAA, RTWA, RTUA Chillers:
- Circuit B - Check AUX3 contact on the 1K6 Run contactor.
- Circuit B - Checking wiring between the 1K6 AUX3 contact and the 1U5 (Compressor B) module input at J3-3,4 (Transition Complete Input).
- Circuit B - Check ALL 1K6 AUX contacts. Check for correct mechanical operation, no binding etc.,..
- Circuit B - Check 1K6 contactor for proper operation.
- Circuit A - Check AUX3 contact on the 1K2 Run contactor.
- Circuit A - Checking wiring between the 1K2 AUX3 contact and the 1U4 (Compressor A) module input at J3-3,4 (Transition Complete Input).
- Circuit A - Check ALL 1K2 AUX contacts. Check for correct mechanical operation, no binding etc.,..
- Circuit A - Check 1K2 contactor for proper operation.
RTAA 130-400 TON Chillers ONLY.
- Verify the P5 menu item 55 is set correctly. If there is a Y-delta starter, item 55 needs to be set to enable. If the the starter is a X-line starter, then item 55 needs to be disabled.
RTAA 70-125, RTUA 70-125, RTWA 70-125 TON chillers ONLY.
- Verify in the Service Settings sub-menu that Reduced Inrush Starting is set to enable for Y-delta start. If the starter is a X-line start, then Reduced Inrush Starting is set to disable.
Notes
- See RTAA IOMs or wiring diagram(s) for reference. (RTAA-IOM-4A or RTAA-SVX01A-EN)
- See RTWA/UA IOMs or wiring diagram(s) for reference. (RTWA-IOM-1A or RLC-SVX07A-EN)
- See also Wave 11252 for additional troubleshooting.
Additional details
Other Question/Problem/Cause Statements
- Failure to Transition...Circuit B? Starter Transition - Compressor B?
- Starter Transition - Compressor A?
- Starter Transition - Compressor B?
- Failure to Transition...Circuit A?
- Transition Fault?
- Compressor sluggish at start...tripping on Transition?
- Intermittent Starter Transition Failure...Compressor A?
- Intermittent Starter Transition Failure...Compressor B?
- Getting 180 and 181 (Starter Transition) Diagnostic.
- Starter transition failure.
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Menu item 55 Reduced Inrush starting is enabled.
- Starter is across the line type, not reduced inrush wye delta type.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.