No communication, Data not valid diagnostic
- If the communication link between the clear language display (CLD) and the control processor module (CPM) is disrupted, the alarm "No Communication, Data not Valid" will be displayed.
- Inspect the interprocessor communication (IPC) link between the two modules, ensuring that the plugs are securely connected.
- Examine the wiring for any breaks and check the plugs for signs of corrosion or poor fit.
- Verify that the IPC link is not incorrectly connected with reversed polarity or to the wrong pins. For example, on the RTAA and RTWA chillers, the 1U2 options module should be connected at J1-1 and 2, not J2-1 and 2.
- A malfunctioning transceiver or other internal component failure may also be the cause of this issue.
Additional details
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.