Condenser Fan Motor Failure / Bearing Wear
Pueblo Technical Support has identified a potential issue in the field with RTAE condenser fan motor (and fan blade) failure.
- Early warning and quality containment has not shown a reliability issue; however, there have been customer chillers where we have seen early or premature failure of condenser fan motors.
- During field investigation we have witnessed condenser fan blades wobbling, indicating a balance issue.
- Field balancing of fans was attempted initially.
- Some fans were able to be balanced.
- Fans that could not be balanced were replaced.
- Until 4-20-2017 fans manufactured could still have an issue with shaft perpendicularity as well as run out. So fans were replaced and had to be balanced
- Further investigation of the motors has shown two other issues:
- Snap Ring is not present in the groove on the motor shaft to hold the fan blade in proper position
- Snap Ring deformation due to improper installation on fan motor shaft
- Bearing/Housing failure can be observed by attempting to move the blade up and down in a vertical motion. If there is movement or a wobble, one or more of the bearings or housing has failed in the motor.
- Investigation of the Fan blade yielded interesting results; where we found the sleeve ( fan blade hub ) not perpendicular to the fan motor shaft, resulting in excessive run-out and no possibility to properly balance the fan-blade, stressing the motor.
See drawings below for reference (notice failure during manufacturing of sleeve/hub installation):
Fan blade Hub/Sleeve: Pass Hub/Sleeve: Fail
Recommended action in the field if fan motor failure occurs
Currently if a fan motor failure occurs due to a balance issue with the fan blade, follow the procedure below:
- If the existing fan blade was manufactured after 4-20-2017 contact Pueblo Technical Support.
Example of date stamp below.
Example date in photo shows: 11-03-2014
- If blade was manufactured prior to this date then replace motor and fan blade.
- Validate new fan blade date code is post 4-20-2017
- Validate Snap Ring is installed properly. The opening in the snap should be 180 degree's away from the keyway groove on the motor shaft.
- Properly torque fan blade bolt. 16 ft-lbs.
Notes
- Fan Motor BLADE Snap Ring (used to support the fan blade and spacing on the motor shaft):
- Missing or improperly placed snap ring results in FAN BLADE rubbing on the orifice.
Fan bolt torque 15 ft.-lbs.
Fan Blade Manufacturer History
- Kenco - Nov 2013 - May 2016
- Kings - May 2016 - Sep 2018
- Lomont - Dec 2018 - Present
Additional details
Other Question/Problem/Cause Statements
- Fan motor failure
- Fan failure
- Condenser Fan Failure
- Motor Failure
- Condenser Motor Failure
Facts
- RTAE (Air Cooled Chiller) - Pueblo
- ACR (Air Cooled Chiller) - Pueblo
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.