What do I need to do to add the 1U2 options module to this chiller?
RTAA, RTWA, RTUA chillers:
- Every RTAA 70-125 unit manufactured in the factory was designed and built with the expectation that the 1U2 Options Module will be installed.
- In cases where the chiller was ordered without the 1U2 module, the power cable (P26) and IPC Communication Cable (P21) will still be included.
- Therefore, it will only be necessary to add the module and connect the cables accordingly.
- For detailed instructions on the location of the connections, please refer to pages 155 (lines 173 & 174) and 157 (lines 233 and 234) of the Installation Operation Manual.
- This module allows for the following features to be utilized:
- External Chilled Water Setpoint
- External Current Limit Setpoint
- Ice Making
- Chilled Water Reset
Contact ABU Modifications (in Lacrosse) for modification direction/information.
Additional details
Other Question/Problem/Cause Statements
- What do I need to do to add the 1U2 options module to this chiller?
- Do I need a special cable for the 1U2 options module?
- Can I add the 1U2 Options Module if it was not built with the chiller?
- Deluxe with Communication Option?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.