What size bolts are used on the water boxes?
- M12 bolts hold the waterbox to the evaporator barrel on all RTAC chillers
- The length of the bolt is dependent upon chiller size
- Those RTAC chillers with 2 compressors will have bolts that are 50 mm long
- Those RTAC chillers with 3 or 4 compressors will have bolts that are 65 mm long
Additional details
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.