Do I need to recover the refrigerant to replace the EXV?
RTAC:
- The refrigerant does NOT need to be recovered to replace the EXV
- The condenser and evaporator are sized such that they are capable of holding the entire charge.
- The recovery equipment can be used to do a liquid transfer from the low side to the high side.
- Close the liquid line angle valve and the discharge service valve prior to moving the refrigerant.
- This procedure would be used if the chiller is not capable of doing a service pumpdown.
Notes
- This is only true for package units as additional refrigerant is needed to compensate for extra piping on remote evaporator units.
Additional details
Other Question/Problem/Cause Statements
- Do I need to recover the refrigerant to replace the EXV?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA)
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.