What is the ice termination setpoint?
The Front Panel Ice Termination Setpoint is the return ice temperature from the ice bank (evaporator entering water temperature).
Front Panel Ice Termination Setpoint can be adjusted from 20°F to 31°F in 1°F increments.
When in the Ice Building mode, and the evaporator entering water temperature drops below the ice termination setpoint, the chiller terminates the Ice Building mode and changes to the Ice Building Complete Mode.
Adequate glycol protection is required to protect the chiller at these temperatures. Use a refractometer to measure the glycol concentration. Use this value to set the Low Evap Refrigerant Temperature Cutout and the Low Leaving Water Temperature Cutout based on the values with the Installation Operation Maintenance (IOM) manual.
Reference the appropriate IOM for more details regarding Ice Making.
Example of warning from IOM:
NOTICE:
Equipment Damage!
Failure to use adequate freeze inhibitor for the leaving water temperature will result in damage to system components.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.