Solid State Starter Conversion bulletin from other types of Solid State Starters (SSS) or Mechanical Starters to Benshaw RediStart Solid State Starter.
- Conversion Bulletin: RLC-SVN005A-EN
- Programming Guide: RLC-SVP001A-EN
- Benshaw SSS Diagnostic and Troubleshooting: RTHD-SVD02A-EN...originally written for MX starters...however most of the information is relevant for MX2 type starters. )
Conversion Tip:
- Recommend providing an external 120VAC to power up the Logic Module for programming, prior to the application of 3-phase power.
- It is recommended that the new starter/logic board be Reset prior to programming.
- Press and hold; PARAM and ENTER on power up to reset the parameters to default values.
Hold PARAM and ENTER buttons until "d f l t" is flashing on the LED display.
Notes
- MX1 and MX2 information is listed in the bulletin.
- November 2011 to present...ONLY MX2 starters are shipped for the conversion.
- See last section of the conversion bulletin for reference on required KIT for converting MX1 Logic Module Starter to MX2 Logic Module Starter. (DO NOT order MX2 Logic Module directly, it will not work. You need to order the KIT listed in the bulletin.)
- If a conversion of logic module has been performed...see appropriate diagrams in conversion bulletin for MX2 wiring.
Useful Motor Information
RTHC / RTHD FLA
| Compressor Code | Nominal Voltage → | 200 | 230 | 380 | 460 | 575 |
|---|---|---|---|---|---|---|
| 60Hz | ||||||
| B1, B2 | 557 | 484 | 291 | 241 | 193 | |
| C1, C2 | 812 | 698 | 421 | 349 | 279 | |
| D1, D2 | 888 | 888 | 549 | 455 | 367 |
| Compressor Code | Nominal Voltage → | 380 | 400 | 415 |
|---|---|---|---|---|
| 50Hz | ||||
| B1, B2 | 233 | 233 | 233 | |
| C1, C2 | 349 | 349 | 349 | |
| D1, D2, D3 | 455 | 455 | 455 | |
| E3 | 488 | 488 | 488 |
RTHA / RTHB FLA
| Model | Nominal Voltage → | 200 | 230 | 380 | 460 | 575 |
|---|---|---|---|---|---|---|
| RTHB 130 | 348 | 302 | 183 | 151 | 121 | |
| RTHB 150 | 390 | 339 | 205 | 170 | 136 | |
| RTHB 180 | 473 | 412 | 250 | 206 | 164 | |
| RTHB 215 | 533 | 471 | 284 | 235 | 188 | |
| RTHB 255 | 629 | 548 | 333 | 275 | 218 | |
| RTHB 300 | 714 | 624 | 378 | 312 | 253 | |
| RTHB 380 | 479 | 395 | 316 | |||
| RTHB 450 | 556 | 460 | 368 |
| Model | Nominal Voltage → | 363 | 380 | 400 | 415 |
|---|---|---|---|---|---|
| RTHB 130 | 174 | 175 | 169 | ||
| RTHB 150 | 216 | 197 | 197 | 190 | |
| RTHB 180 | 263 | 238 | 239 | 240 | |
| RTHB 215 | 299 | 270 | 271 | 270 | |
| RTHB 255 | 347 | 313 | 314 | 314 | |
| RTHB 300 | 398 | 360 | 361 | 361 | |
| RTHB 380 | 499 | 479 | 475 | 476 | |
| RTHB 450 | 584 | 561 | 558 | 555 |
Additional details
Other Question/Problem/Cause Statements
- Benshaw SSS Conversion?
- Cutler Hammer Solid State Starter Conversion?
- A515 Solid State Starter Conversion?
- C515 Solid State Starter Conversion?
- S801 IT Solid State Starter Conversion?
- S811 IT Solid State Starter Conversion?
- Benshaw Solid State Starter Conversion?
- Solid State Starter Conversion?
- Wye Delta Starter Conversion?
- Benshaw MX Logic Module Failure?
- MX1 Logic Module Failure?
- How to convert to MX2 Logic Module?
- How to convert Benshaw MX to MX2 Solid State Starter?
- Benshaw Logic Module Failure?
- Benshaw Solid State Starter Logic Module Failure?
- Y-Delta Starter Conversion?
- Mechanical Starter Conversion?
- MX to MX2 Conversion?
- Benshaw Solid State Starter MX to MX2 conversion?
Facts
- CenTraVac - Direct Drive Simplex (CVHE, CVHF, CVHG)
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTHD)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.