What is the sensor depth?
If sensors need to be replaced and new sensors are available: the new sensor can be taped/strapped on to the existing refrigerant lines and connected to the chiller controls. Pumpdown then may be initiated using the external sensors for control. This is only for help in speeding up the refrigerant handling process and is not recommended for permanent installation.
Once the chiller has been pumped down, perform standard refrigeration recovery practices. Remove and replace the sensors, set to the correct sensor depth.
Drawings listed below are attached at the bottom of this article.
- See attached drawing for RTAA 70-100 chillers (180401H.pdf).
- See attached drawing for RTAA 110-125 chillers (174001H.pdf).
- Sensors are direct immersion type...in the refrigerant/oil.
- See attached drawing for RTAA 130-215 reference. (902601A.pdf)
- See attached drawing for RTAA 240-300 reference. (114700C.pdf)
- See attached drawing for RTAA 340-400 reference. (902301A.pdf)
Sensors are direct immersion type...in the refrigerant/oil.
Additional details
Other Question/Problem/Cause Statements
- What is the sensor depth?
- Liquid line sensor depth?
- Temperature sensor depth?
- Suction sensor depth?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.