In April of 2018, there was a design sequence change for RTAF chillers.
- The design sequence changed from AE to AF (digits 10 and 11 in the model number).
- What changes are associated with the design change?
- The Bray actuated suction valve has been removed and replaced with a manual suction service valve pressure transducers 3BP5 and 4BP5 have been removed
- receiver tanks have been added to each circuit and solenoids 3M25 and 4M25 have been added.
- The 115 ton - 215 ton RTAF chillers now utilize receiver tanks & solenoid valves, like the 230 ton to 500 ton RTAF chillers do for managing refrigerant with reduced internal condenser volume (MCHE).
- The RTAF Electrical Packages that ship with the chiller are being updated, but currently don't include the design sequence AF changes.
Please see the attached marks up for both the Refrigerant and Oil System Schematic, and the Electrical Schematics.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.