Do we have IFM Efector Flow Switch Information
Efector Flow Switch Information: Information regarding the programmer tool can be found in this document.
- IFM Programming Tool - attached below as ifm __ EVC070.pdf
- Programming Cable - attached below as ifm __ EVC070.pdf
Programming
The following programming steps will ONLY work with TestPak E18401. Do not attempt the programming using TestPak E18430.
- Programming can be done in flow or no-flow conditions
- After connecting the battery box to the SC0505, the Testpak will respond with a 15 second output
- The use of a clock timer for programming is recommended.
- Press the teach button (red button) for 5 seconds
- Release the teach button for 5 seconds
- Press the teach button again for the desired switch-point/velocity (60 seconds for 60/s; 15 seconds for 15 cm/s, etc..)
- Release the teach button. After 5-second delay:
- With no flow, the SC0505 will respond with an equivalent output (ex. 60 seconds for 60 cm/s).
- With flow, the SC0505 output will turn off for an equivalent time (ex. 60 seconds for 60 cm/s)
- After 5 seconds, the sensor returns to monitoring mode. The switch-point/velocity is adjusted.
Velocity
There are five (5) different velocities available (all files attached below)
- X13790871010 >>> 15 CM/S (Green - label) - SC0522
- X13790871020 >>> 35 CM/S (White - label) - SC0523
- X13790871030 >>> 45 CM/S (Yellow - label) - SC0524
- X13790871040 >>> 60 CM/S (Orange - label) - SC0525
- X13790871050 >>> 25 CM/S (Lt. Blue - label)
See programming steps above to program the required velocity into the switch.
PART NUMBERS SHOULD BE VERIFIED BY TRANE PARTS
It can be re-programmed if their service company has the tool. If they do, then they will have to mark the sensor that it has the new setting for future reference.
OR
If the customer does not have the tool, then they can just order a new flow switch that has the correct setting on the sensor.
Additional details
Other Question/Problem/Cause Statements
- IFM Efector Flow Switch Programming?
- Is there a procedure to program the IFM Efector Flow Switch?
- Can the flow switch be programmed?
- Programming the IFM Efector Flow Switch?
- Can the electronic flow switch be programmed?
- How do I wire the programmer for the IFM flow switch?
- Wiring for the IFM flow switch programmer?
- Efector Flow Switch?
- What color flow switch should I have?
- Do I have the correct flow switch for my chiller?
- IFM Efector Programming
Facts
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
- Compressor Chiller (Pueblo) (RTUD 70-200 Ton)
- Water-Cooled Chiller (Pueblo) (RTWD)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Air-Cooled Chiller (Pueblo) (RTAE)
- Air-Cooled Chiller (Pueblo) (RTAF)
- Air-Cooled Chiller (Pueblo) (ACRA)
- Air-Cooled Chiller (Pueblo) (ACSA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.