Table of Contents
Wiring and Setup: Symbio Condenser or Heat Pump with SZVAV / 2 Speed Air Handler
Look at the bottom of this article for a downloadable copy
Condenser: Odyssey Condenser with Symbio 700 Controls
AHU: Odyssey AHU with Symbio control boards and model number digit 15 = D
Symbio 700 Quick Links
- Symbio™ 700 - Where to download the Service & Installation Mobile Phone App
- Symbio™ 700 - Bluetooth Connection Instructions
- Symbio™ 700 - Precedent or Odyssey - How to configure or edit configurations using the Mobile Phone App
How many wires do I need?
1 - Up to 7 conductor thermostat wires between the thermostat OR zone sensor and condenser
1 - Up to 6 conductor control wires between the AHU and condenser
2 - 2-conductor twisted, shielded, stranded communication wires between the AHU and condenser.
Cable Identification
Field Wiring
AHU Wiring to Condenser
Cable #1 Modbus Communication
Cable #1 is a Modbus communication link between Symbio 700 and the AHU VFD. It is required for Pairing B as the AHU uses a communicating VFD. This cable must be a 2-conductor, twisted, shielded, stranded cable intended for 2 wire communications. We recommend Trane Purple Comm wire (Windy City Wire Spec #0523003) or any 2 conductor comm wire. 3 Conductor comm wire is also acceptable for Cable #1. Symbio Communication Wire
DO NOT USE THERMOSTAT, ETHERNET OR NON-COMMUINCATION RATED WIRE FOR COMMUNICATIONS
AHU Wiring to Condenser
Cable #2 Control Wiring
AHU Wiring to Condenser
Cable #3 IMC Communications
Cable #3 is an IMC communication link between Symbio 700 and the Indoor Option Module. It is required for electric heat operation and VVZT configuration. This cable must be a 2-conductor, twisted, shielded, stranded cable intended for 2 wire communications. We recommend Trane Purple Comm wire (Windy City Wire Spec #0523003) or any 2 conductor comm wire. Symbio Communication Wire
DO NOT USE THERMOSTAT, ETHERNET OR NON-COMMUINCATION-RATED WIRE FOR COMMUNICATIONS
Wiring Thermostat to Condenser
Cable #4A Thermostat Wiring
Cable #4A is for conventional thermostat use or when the condenser is controlled by relays. Unit will only use Cable #4A or 4B, not both.
Wiring Zone Sensor to Condenser
Cable #4B Zone Sensor Wiring
Cable #4B is for zone sensor use and is required when VVZT (SZVAV) operation is desired. Zone sensors are commonly used with BAS or can be standalone. Unit will only use Cable #4A or 4B, not both.
*Zone sensor wiring shown for BAYSENS135, other mechanical zone sensors similar.
Emergency Stop Wiring
From Stop Devices to Symbio 700
Wiring above reflects normally closed safeties. Typically, condensate overflow switches (or pan switches) are normally closed devices. If using normally open devices, they can be wired in parallel, and the Customer Connection Polarity does not need to be changed.
For more information, see the links below:
- Trane Commercial Help Center - Symbio™ 700 - Emergency Stop Input
- Trane Commercial Help Center - Symbio 700 Demand Limit and Emergency Stop Polarity
Configuring Symbio 700
Odyssey condensers can be paired with many different Odyssey AHUs, 3rd party AHUs, and indoor coil assemblies. Due to this, Symbio 700 must be configured for the connected AHU, installed accessories, and the controlling sensor/thermostat.
Configuring Link from Trane Commercial Help Center
Phone Application
Onboard Display
Tracer TU
VVZT Configuration Needed
For Variable Volume Zone Temperature (VVZT or formerly known as SZVAV) operation, set the configuration as follows (requires zone sensor):
- System Type = VVZT (requires zone sensor for actual VVZT operation, tstat will operate as CVZT)
- Efficiency = Standard B
- Indoor Fan Type = Variable Speed (should set automatically)
- Space Controller = Single Setpoint Zone sensor, or Dual Setpoint Zone Sensor
- Frostat = Installed (should install automatically) + (On Odyssey, this is the high limit for the VFD)
- Discharge Temperature Sensor = Installed (should install automatically)
-
Field-installed electric heat only
-
TTA condenser
- Primary Heating Source = Electric
- Primary Heating Stages = 1 or 2 (depending on electric heat kit stages)
-
TWA condenser
- Primary Heating Source = Heat Pump
- Primary Heating Stages = 1 or 2
- Secondary Heating Source = Electric
- Secondary Heating Stages = 1 or 2 (depending on electric heat kit stages)
-
TTA condenser
Multispeed Configuration Needed
For Multispeed fan operation, set the configuration as follows:
- System Type = CVZT (thermostat or zone sensor)
- Efficiency = Standard B
- Indoor Fan Type = Multi Speed
- Space Controller = Conventional Thermostat, Single Setpoint Zone sensor, or Dual Setpoint Zone Sensor
- Frostat = Installed (On Odyssey, this is the high limit for the VFD)
- Discharge Temperature Sensor = Installed (with zone sensor, will use DAT logic for compressor staging) or Not Installed for conventional thermostat.
-
Field-installed electric heat only
-
TTA condenser
- Primary Heating Source = Electric
- Primary Heating Stages = 1 or 2 (depending on electric heat kit stages)
-
TWA condenser
- Primary Heating Source = Heat Pump
- Primary Heating Stages = 1 or 2
- Secondary Heating Source = Electric
- Secondary Heating Stages = 1 or 2 (depending on electric heat kit stages)
-
TTA condenser
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.